Hi:
I tried sending to the suggested address for the CCS4 Beta support team but DAEMON just bounced the e-mail so I do not know what to do next. Help is appreciated, even if just a correct e-mail address that goes somewhere.
I'm doing the tutorials on program setup and have gotten to the point of loading the 'Volume1' program to the target.
The target has previously run the 'Blink' program fine under CCS3.3 and this computer. 28027 control stick also ran 'Blink' fine with this computer and CCS3.3.
I'm using Windows XP on a new ASUS laptop. The XP is fully updated.
I have not had any previous beta of CCS4 in my computer, just limited CCS3.3. I didn't remove 3.3 in any way.
I'm connected to a TMDXDOCK28027 Piccolo A experimenters kit. I seemed to connect ok to the computer as it was recognized and the CCS 4 (CCS3.3 platinum= CCS4?) seems to run ok.
I downloaded CCS4 from the TI website, beta. Download went smoothly.
That's what I've got running. Everything has gone ok to this point, the tutorial is good and reasonable and I was doing fine until this hit so it will be interesting to see what has gone wrong.
I seem to have done everything right so far and the Project View looks as it does in the example.
When I build the program I get:
1error one or more sections of your program falls into a memory region that is not writeable---
Loading Program requester says:
...cfs/volume1/volume1/Debug/volume1.out
loading sections
a window here stays empty. Below it appears this:
.reset 0 of 4 at 0x3fffc0
An error window pops up with:
Data verification failed at address 0x3fffc0
Please verify target mem and mem map.
---------
(end of problem statements)
Since I'm doing a tutorial to learn how to use this setup I don't yet know how to verify my target mem so I don't know what to do to solve the problem. I'm not sure I would understand the result if verifying it didn't clearly tell me what I might do to correct the situation when it tells me what's wrong.
I've checked the forum and your wiki and do not see an answer anywhere.
I haven't tried to migrate any previous programs or any other activity besides just starting the tutorial.
Thanks for your help
Larry Grant