This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320LF2407A and CCS V4 build error

Now I am entering in CCSv4 and still had some questions.

I start a new project, include them files, in the settings are different build configuration but my problem is the following :
When I compile a file (all code is in assembler) it returns errors (E0003 and E0002) for an included file (LF2407.h) witch contain processor register symbols attributions. That should mean that the used compiler does recognize in this case the "IFR" string as a keyword. I found on the install dir a specific compiler for C2400 but I am unable to made the system discover it with the correct discovery path. The problem is with c2000 compiler ver 5.0.2 and I will use the C2400 compiler version 7.04 (that we use in version 3.3 of ccs) ?
Any idea ?

Another point is that the import wizard "import legacy CCSv3 project" goes not further after selecting the .pjt file. I can click on the Next button but no changes! the destination folder (workspace) is empty. The "copy project into workspace" flag was set.

I am on PC (core 2 duo, E7300 2GB RAM) with winXP SP3
The computer is completly new and fresh installed.

These questions were allready sent to EPIC (Europe) and transmitted to the CCSV4 survey since more than 2 weeks without any feedback !

Thanks in advance for help.

These questions were allready sent to EPIC (Europe) and transmitted to the CCSV4 survey since more than 2 weeks without any feedback !

Thanks in advance for help.