This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SCI Booting tms320f28335

i have converted the .out file of examples given in TIdcs to intel hex files using hex2000 utility. i tried to program these files using c2000prog. but it shows SECTOR VIOLATION error. could anyone help me?

my cmd file:

 

 

MEMORY

{

PAGE 0 :

   /* BEGIN is used for the "boot to SARAM" bootloader mode      */

   /* BOOT_RSVD is used by the boot ROM for stack.               */

   /* This section is only reserved to keep the BOOT ROM from    */

   /* corrupting this area during the debug process              */

   

   BEGIN      : origin = 0x000000, length = 0x000002     /* Boot to M0 will go here                      */

   BOOT_RSVD  : origin = 0x000002, length = 0x00004E     /* Part of M0, BOOT rom will use this for stack */               

   RAMM0      : origin = 0x000050, length = 0x0003B0

 

   RAML0      : origin = 0x008000, length = 0x001000    

   RAML1      : origin = 0x009000, length = 0x001800    

   RAML2      : origin = 0x00B000, length = 0x001000    

   RAML3      : origin = 0x00C000, length = 0x001000 

   ZONE7A     : origin = 0x200000, length = 0x00FC00    /* XINTF zone 7 - program space */ 

   CSM_RSVD   : origin = 0x33FF80, length = 0x000076     /* Part of FLASHA.  Program with all 0x0000 when CSM is in use. */

   CSM_PWL    : origin = 0x33FFF8, length = 0x000008     /* Part of FLASHA.  CSM password locations in FLASHA            */

   ADC_CAL    : origin = 0x380080, length = 0x000009

   RESET      : origin = 0x3FFFC0, length = 0x000002

   IQTABLES   : origin = 0x3FE000, length = 0x000b50

   IQTABLES2  : origin = 0x3FEB50, length = 0x00008c

   FPUTABLES  : origin = 0x3FEBDC, length = 0x0006A0

   BOOTROM    : origin = 0x3FF27C, length = 0x000D44               

         

PAGE 1 : 

   RAMM1      : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */

   RAML4      : origin = 0x00C000, length = 0x001000    

   RAML5      : origin = 0x00D000, length = 0x001000    

   RAML6      : origin = 0x00E000, length = 0x001000    

   RAML7      : origin = 0x00F000, length = 0x001000 

   ZONE7B     : origin = 0x20FC00, length = 0x000400     /* XINTF zone 7 - data space */

}

 

 

SECTIONS

{

   /* Setup for "boot to SARAM" mode: 

      The codestart section (found in DSP28_CodeStartBranch.asm)

      re-directs execution to the start of user code.  */

   codestart        : > BEGIN,     PAGE = 0

   ramfuncs         : > RAML0,     PAGE = 0  

   .text            : > RAML1,     PAGE = 0

   .cinit           : > RAML0,     PAGE = 0

   .pinit           : > RAML0,     PAGE = 0

   .switch          : > RAML0,     PAGE = 0

   

   .stack           : > RAMM1,     PAGE = 1

   .ebss            : > RAML4,     PAGE = 1

   .econst          : > RAML5,     PAGE = 1      

   .esysmem         : > RAMM1,     PAGE = 1

 

   IQmath           : > RAML1,     PAGE = 0

   IQmathTables     : > IQTABLES,  PAGE = 0, TYPE = NOLOAD 

   IQmathTables2    : > IQTABLES2, PAGE = 0, TYPE = NOLOAD 

   FPUmathTables    : > FPUTABLES, PAGE = 0, TYPE = NOLOAD 

      

   DMARAML4         : > RAML4,     PAGE = 1

   DMARAML5         : > RAML5,     PAGE = 1

   DMARAML6         : > RAML6,     PAGE = 1

   DMARAML7         : > RAML7,     PAGE = 1

   

   ZONE7DATA        : > ZONE7B,    PAGE = 1  

 

   .reset           : > RESET,     PAGE = 0, TYPE = DSECT /* not used                    */

   csm_rsvd         : > CSM_RSVD   PAGE = 0, TYPE = DSECT /* not used for SARAM examples */

   csmpasswds       : > CSM_PWL    PAGE = 0, TYPE = DSECT /* not used for SARAM examples */

   

   /* Allocate ADC_cal function (pre-programmed by factory into TI reserved memory) */

   .adc_cal     : load = ADC_CAL,   PAGE = 0, TYPE = NOLOAD

     

}

 

SECTIONS

{

Net_terminals: > RAML4,PAGE = 1

Controller: > RAML4,PAGE = 1

IBx_addr: > RAML4,PAGE = 1

Buck1Loop: > RAML4,PAGE = 1

Buck2Loop: > RAML4,PAGE = 1

DataLogTST: > RAML4,PAGE = 1

GraphData: > RAML4,PAGE = 1

}

 

 

Thanks in advance

malaiyappan,m

  • Hi Malaiyappan,

    You declare in Page 0:

    RAML3      : origin = 0x00C000, length = 0x001000

    and in Page 1:

    RAML4      : origin = 0x00C000, length = 0x001000

    I guess you know this cant be good :)

     

    Also a minor fix to get more RAML1 space

      RAML1      : origin = 0x009000, length = 0x001800  

       RAML2      : origin = 0x00B000, length = 0x001000   

    You can set the length of RAML1 to 0x002000 , unless you had other plans with that space

    Leo