Other Parts Discussed in Thread: CCSTUDIO, TMS320F28335
I have the 28335 Experimenter's Kit and am having trouble figuring out how to configure a project for the '335 using DSP/BIOS. Is there an app note somewhere detailing how to create and build a DSP/BIOS project for the '335 with hardware floating point support? I am having a lot of trouble figuring which libraries to include, etc. I am just not finding much documentation on getting the floating point 283xx parts up and going. Here's the result of my latest attempt:
<Linking>
fatal error: file
"C:/CCStudio_v3.3/bios_5_33_03/packages/ti/bios/lib/lnkrtdx.a28FP<rtdx.o28FP
>" specifies ISA revision "C28FPU32", which is not compatible with ISA
revision "C2800" specified in a previous file or on the command line
>> Compilation failure
Any help would be greatly appreciated!
John