hi all,
i have ezdsp f28335,so i want to use xintf zone 6 for my external memory. my C-code is:
in linker comand file
MEMORY
{
.....
PAGE 1 :
ZONE6 : origin = 0x100000, length = 0x000003 /*XINTF zone 6 - data space 3x16*/
............
}
SECTIONS
{
........
ZONE6DATA : > ZONE6, PAGE = 1
}
In mainfile C-code:
#define BUF_SIZE 3 // Sample buffer size for 3 duty cycle
#pragma DATA_SECTION(Buf , "ZONE6DATA" );
volatile Uint16 Buf[BUF_SIZE]; // i dont know whether i must use keyword "volatile" or not ?
.........
//so in ISR(interrupt service routine) :
........
intterupt void main_isr(void)
{
...........
...........
BUF[0] = (Uint16)(....);
BUF[1] = (Uint16)(....);
BUF[2] = (Uint16)(....);
..........
}
question is : is it right???
For the first assignment BUF[0], so addressline A1 = 0 and A0 = 0, WE = 0, CS = 0
For the 2nd assignment BUF[1], so addressline A1 = 0 and A0 = 1, WE = 0, CS = 0
For the third assignment BUF[2], so addressline A1 = 1 and A0 = 0, WE = 0, CS = 0
many thanks!
tequila