This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS v5 won't work with picolo F28069 control stick

Other Parts Discussed in Thread: CONTROLSUITE, TMS320F28069

I'm trying to do the first CCS workshop (blinking LED) and nothing works because the project was written for CCS v4.  I think I finally got the compiler changed from version 5.x to 6.x, but there are still errors.  What do I need to do to make this work?  Here's what I get:

 

**** Build of configuration F2806x_FLASH for project BlinkingLED ****

C:\ti\ccsv5\utils\bin\gmake -k all 'Building target: BlinkingLED.out' 'Invoking: C2000 Linker' "C:/ti/ccsv5/tools/compiler/c2000_6.1.0/bin/cl2000" -v28 -ml -mt --cla_support=cla0 --float_support=fpu32 --vcu_support=vcu0 -g --define="_DEBUG" --define="LARGE_MODEL" --define="FLASH" --diag_warning=225 -z --stack_size=0x300 -m"BlinkingLED.map" --warn_sections -i"C:/ti/ccsv5/tools/compiler/c2000_6.1.0/lib" -i"C:/ti/ccsv5/tools/compiler/c2000_6.1.0/include" -i"C:/Users/Don/workspace_v5_1/TMS320F28069_controlSTICK/BlinkingLED" --reread_libs --rom_model -o "BlinkingLED.out"  "C:/ti/controlSUITE/device_support/f2806x/v100/F2806x_headers/cmd/F2806x_Headers_nonBIOS.cmd" "./F2806x_GlobalVariableDefs.obj" "./F2806x_CodeStartBranch.obj" "./BlinkingLED-Main.obj" "./BlinkingLED-DevInit_F2806x.obj" -l"rts2800_ml.lib" "../F2806x_FLASH_BlinkingLED.CMD" <Linking> error: file    "C:/ti/ccsv5/tools/compiler/c2000_6.1.0/lib/rts2800_ml.lib<boot.obj>"    specifies ISA revision "C2800", which is not compatible with ISA revision    "C28FPU32" specified in a previous file or on the command line error: file

   "C:/ti/ccsv5/tools/compiler/c2000_6.1.0/lib/rts2800_ml.lib<exit.obj>" >> Compilation failure    specifies ISA revision "C2800", which is not compatible with ISA revision    "C2700" specified in a previous file or on the command line error: file    "C:/ti/ccsv5/tools/compiler/c2000_6.1.0/lib/rts2800_ml.lib<_lock.obj>"    specifies ISA revision "C2800", which is not compatible with ISA revision    "C2700" specified in a previous file or on the command line error: file    "C:/ti/ccsv5/tools/compiler/c2000_6.1.0/lib/rts2800_ml.lib<args_main.obj>"    specifies ISA revision "C2800", which is not compatible with ISA revision    "C2700" specified in a previous file or on the command line error: errors encountered during linking; "BlinkingLED.out" not built gmake: *** [BlinkingLED.out] Error 1 gmake: Target `all' not remade because of errors.

**** Build Finished ****