Hi Everyone,
I am building a basic platform upon which I can create my 28335 application. I'd like to start with a console application that allows input/output to a serial port (via SCI).
I will need this since I will not always have CCS connected. I started with Example_2833xSci_EchoBack.c. I added a printf() statement and, of course, it appeared in the Stdout window in CCS.
My question is.....How do I connect the basic I/O functionality of the Echoback example so that printf() scanf() is connected to it and these functions talk to the serial console?
I guess one way is to create a device driver for the SCI and then use fscanf() and fprintf() and the appropriate fopen() calls beforehand but
I was hoping there would be an easier way.
Thanks,
Victor from VisualCue Development