This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

sizeof() method used on struct

I have read that the method sizeof(char) will return 1 and sizeof(int) will also return 1 since the F28335 can only address 16 bits values.

I have trouble understanding how the sizeof method is implemented in CCS.  For example, I run the following code:

struct sVarsStorage
{
    int16       id;             // Var Id
    float32     value;     // Var value
};

Uint16 lIntSize = sizeof(int16);

Uint16 lFloatSize = sizeof(float32);

Uint16 lBufEntrySize = sizeof(sVarsStorage);


And obtain the following:

lIntSize = 1 as expected.

lFloatSize = 2 as expected.

lBufEntrySize = 4 ??? (I would have expected 3!)

What will happen if I use a char* to compute the CRC of a table of n elements of type sVarsStorage?