|
Hi all, When using the ePWM module of the F28335 chip to output sinusoidal PWM wave to drive three phase full bridge IGBTs, I would like to know when can I update the value of counter-compare register CMPA and CMPB? Can I update it at any moment I want? In addition, when the TBCTR register is non-zero and is decreasing, I clear the TBCTR register to zero, will the TBCTR register downwards overflow? thanks a lot! |