Hello.
Is there any good primer or user guide that can give me enough insight on how the I2C peripheral works? I have read the complete documentation many times and looked to several examples, but still some of the information is confusing. For example, sometimes when I configure the module as a receiver the MST bit changes from 1 to 0, though AL is unaffected. Also, it has happened to me that the module goes into a numb state and it does not respond to an IRS reset; only a power cycle will clear it. It seems it is very sensitive to the order of operations.
Regards.