We have been using the 2407A for a few years and have always used the ADC at "full" speed (40MHz)(CPS = 0 and ACQ bits 0) with no apperant problems.
We are now updating our controller and sampling more channels and upon review of the TI ADC doumentation SPRS145J (datasheet) and SPRU357C (manual) there is some confusion about the ADC clock speed. The datasheet states that the clock cannot be greater than 30MHz but the manual uses examples using the 40MHz clock rate. The datasheet limitation tells me that the ADC cannot run at 40MHz and that the clock will have to be divided down.
Does this mean that CPS has to equal 1 for the 2407A so that the clock will now be 20MHz and is slower than the minimum cycle time of 33.3ns?
Also when I set CPS = 1 and leave the ACQ bits = 0 the ADC does not operate (all channels read a rail value). If I set CPS = 1 and ACQ bits to any value greater than 0 the ADC works properly.
Thanks in advance for any clarification on this,
Russ