Other Parts Discussed in Thread: TMS320F2808
Hi!
I am designing a board with F2808. Reading the TI's pdfs it is clear that the only two ways to power the DSP are:
1. to power both rails (3.3 V, 1.8 V) together or
2. ramp 1.8 V rail before 3.3 V rail in order to get glitch free power-up on GPIO pins.
Why do all the solutions (ezDsp schematic, recomendend power soulutions availabile on TI's swebsite) do the oposite - first ramp up 3.3 V rail and then ramp aup 1.8 V rail.
Any comments, experiences are welcome.
Regards, Mitja