Other Parts Discussed in Thread: CCSTUDIO
It is possible to run the SDFlash tool from the command line of Windows?
Or it is possible to embed the tool in a user application programmed with C/C++?
Thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CCSTUDIO
It is possible to run the SDFlash tool from the command line of Windows?
Or it is possible to embed the tool in a user application programmed with C/C++?
Thank you!
Sebastien,
I have never seen an option or any documentation that explains if you can run this tool from command line. You may want to contact Spectrum Digital directly regarding this. As far as embedding the tool into user application, the source code is not provided for the SD Flash Gui so you do not have access to the code to automate this. I assume this is what you are attempting to do.
Regards,
Tim Love
Thank you Tim for your response!
I searched in the web and found that there is an xmlgui application from Spectrum Digital. When you install this application, there is a example project in the folder
CCStudio_v3.1\specdig\sdtsrv\Examples\eZdsp2000\Test28xmfc
Here the source code is provided....
Regards,
Sebastian