This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Xtal 14.7456MHz on Launchpad C2000

Good Morning Friend. Then I'm working on Piccolo lauch pad and I need change a speed of processor using a crystal. I pretend use  a 14.7456MHz, with informations of GEL CCS 3.3 , if I set PLLosc to multiply 12/2 I will have 58,98MHz. I would like some one say what parameters I need chenge on program to work with this speed . 

Thanks everyone