This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello!
Does anyone knows if I can combine the TMS320F2812 eZdSP SYSTEM KIT and DMC550 Motor Controller to control an brushless motor? In the DMC550 Motor Controller documentation it only refers to eZdsp LF2407 and F240, F243, LF2407 DSP Starter Kit (DSK).
Thank you!
You can use the DMC550 with the 2812 eZdsp. We have an example PMSM solution that uses the DMC550 board with the 2812 eZdsp. You can download this from the following link:
http://focus.ti.com/docs/toolsw/folders/print/sprc179.html Regards, Tim Love
Hello Tim Love,
I have the 2808 eZdsp kit and the DMC550 board. And I'm trying to run a simple program from TI documents but can't run it.
Do you have a detailed simple steps to use these parts as a power inverter? Just a simple program to use this kit.
Thanks,
Joe
Hello Jim,
It's been a long time for me looking for any reference in running both the f2808 eZdsp and DMC550 as an inverter. Do you have any documents in running these kits? I'm using CCS v 3.1.
Thanks in advance.
Joe