Other Parts Discussed in Thread: SPRC191
Hello
I have an application on a F2802 with CAN, I2C (EEPROM) and some GPIOs.
After the initialisation i read data from the EEPROM and transmit a CAN message.
If i read the data from the EEPROM and GPIO22 (configured as input) is high,
then the CAN message can not be sent.
When the input is low or i dont read the data before sending a CAN message
it works.
Can someone explain me that strange phenomenon?
Greets
Philipp