Other Parts Discussed in Thread: TMS320C28346
Hi,
I've been working with the eCAN modules in a TMS320C28346 at
a speed of 1Mbps with no problems, but lately I was testing higher
speeds (2Mbps, 3Mbps, etc.), and the module seems to work up to 3Mbps.
I know that the standard indicates that 1Mbps is the limit, however I
think that at short distances and using only TMS320C2x microcontrollers
I do not see a major problem for using higher speeds. Anyway my
questions are: what is the maximum speed that you have tested for this
module?, do you think that these speeds could be used in real world
applications?
Thanks for your help,
Paul Vicioso