Hi,
I just installed the newest TI Resource explorer. I found there the project PM_Sensorless for DRV8301-HC-Kit. Is there also a project for a sensored (hall-sensors) application available? The hardware is designed to do that. I know, that there is a sensored applicaticon for the DRV8412-C2-Kit. But I would like to have one for the Piccolo F28035 with a high power ouput stage (24V / 60A -> DRV8301-HC-C2-Kit).
Best regards
Uwe Schoch