I was trying to configure external clock (XCLKIN) on F28069 on GPIO19 (Pin 52 on 80-pin PN package; GPIO19 multiplexed with XCLKIN). I'm using F28069 USB controlSTICK. The schematic shows that X2 has been left open, while X1 is grounded. GPIO19 is brought out on pin 25 on J1 header. I've tested the external 12MHz resonator (getting power from pin 32-Ground and pin 4-3V3). The resonator output is ok. The intent is to disable and bypass PLL, and directly use external clock. Unfortunately, I haven't had any success so far in configuring XCLKIN as the system clock.
Has anyone tried that? Maybe I'm doing something wrong, so it would be nice for someone to share system clock configuration with me. Even though this device is not a part of any of my current projects, it will block me from considering it for any of my future projects. My preference will be to use GPIO19 rather than GPIO38 (Pin 54 on 80-pin device) for external clock.
Thanks
-Ahmad