This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem using watchdog to wake up from standby

Hi all,

I want to use the watchdog to periodic wake up from standby, check the adc and then go back to sleep. 

The watchdog is set to WAKEINT and works when system is not in standby. 

I can wake from standby by pressing a button attached to GPIO14.

I have tried executing the code with and without the debugger attached and there is no difference.

What am i missing?

My standby procedure looks like this:

void LPM_gotoSleep(void)

{

// The wakeup signal should be (2+QUALSTDBY) OSCCLKs wide.
SysCtrlRegs.LPMCR0.bit.QUALSTDBY = 0;

// enable watchdog in standby
SysCtrlRegs.LPMCR0.bit.WDINTE = 1;

EALLOW;

GpioIntRegs.GPIOLPMSEL.all = 0;

// Wake up on control panel press
GpioIntRegs.GPIOLPMSEL.bit.GPIO14 = 1;

if (SysCtrlRegs.PLLSTS.bit.MCLKSTS != 1) // Only enter Standby mode when PLL is not in limp mode.
{
// Write the LPM code value
SysCtrlRegs.LPMCR0.bit.LPM = 0x0001; // LPM mode = Standby
}
EDIS;

// use watchdog to periodic wake from sleep

SysCtrlRegs.WDCR = 0x002F;
WDT_reset();

EALLOW;

SysCtrlRegs.CLKCTL.bit.WDCLKSRCSEL = 1;    // Switch Watchdog Clk Src to external

EINT; // Global Enable all Interrupts

// Force device into STANDBY

asm(" IDLE");

}