Other Parts Discussed in Thread: CONTROLSUITE
Hi, im currently designing a custom Board with a F28069 and im a little bit confused reading the Design Guidelines for the Oscillator Designs.
It is said, that there are two ways of configuration: internal with a crystal and two capacitors and external with an external oscillator.
First Question (internal configuration) :
-Are the capacitors (C1, C2, see the picture below) real capacitors and i have to use on the board design or are they for substituton of the crystal curcuit? do they have to be a special kind of capacitors (are ceramic caps working) ?
-CLoad has to be around 12pF. So if im picking two capacitors depending on the equation in wich capacity range/area do the caps have to be ? also pF? nF? or higher?
-The crystal has to be chosen also with 12pF, right?
-Will the USB Module and the Serial interfaces work with this configuration? i found some posts saying that the internal configuration is a bad choice for the serial interfaces but im not sure wich configuration is meant.
-What is the device doing if you leave the pins unconnected? just out of curiosity.
One more for the external Configuration:
Do you know any good Design Guidelines for designing an external Oscillator curcuit? Couldnt find some in controlSuite/internet yet.
Thanks a Lot!