Dear Champs,
One of my customers is powering the F281x according to the datasheet recommendations.
However, there is no slew rate statement on the 3.3V rail in the datasheet. On their board it may happen that the 3.3V supply is rising very slow, and it is also possible that the voltage is staying on a certail level in between 0V and 3.3V for an extended time depending on some environment conditions. So far they have not experienced issues with it.
Their question is: Do they have to expect issues long-term? Do we have recommendations for this?
Thanks!
Best regards,
Andreas