Hi Guys,
I have a customer who is permanently damaging (blowing) the F2811 DSP when attempting to program the FLASH the JTAG. So far he has damaged 6 parts on different PCBs. He tried using a different emulator and also a different PC but the problem still occurs.
If he manages to succesfully progam the FLASH, the DSP works properly and doesn't "blow". He's working in a anti-static controlled environment and has used other C2000 parts and the same programming environment successfully for the past 5 years without any problems. The DSP is powered via a TPS767D301PWP LDO, also a tried and tested implementaion.
I was able to find out that he doesn't stick to the recommended power up sequence and is ramping up 1.8V and 3.3V simultaneously, could this cause such problems?
The parts affected are all G revision.
Thanks in advance,
Magnus