I have a Concerto f28m35x control card. Using v150 of the Control Suite, I'm trying to get both the blinky_dc_m3 and blinky_dc_c28 code to blink after resetting the control card's power supply. I am loading both of them in flash. I have all the setting switches in SW1 in the down position. When I cycle power, the m3 blinky does work with no debugger attached. However, the c28 blinky only works right after being loaded in the debugger. I saw another thread here that implied simply adjusting the SW1 switches would solve this problem and allow the c28 to boot from flash. Is there some other configuration I should be using or a line of code that is not included in the examples?