This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SEQ1/2_BSY register on F281x



Hi champs,

My customer is aware of the INT_SEQ1/2 errata on F281x devices. They are not using the INT_SEQ1/2 registers but SEQ1/2_BSY regs instead. They are wondering if the same 1 extra cycle delay will apply to the SEQ1/2_BSY since they are not using INT_SEQ1/2.

Thanks,

 Maite

  • Hi again,

    Regarding the question below, since the errata only talks about INT_SEQ1/2, can I assume that they don't need to consider any extra delay if they are not using the specified register?

    Cheers,

    Maite 

  • Maite,

    This is correct, there is no errata concerning the BSY bits.  Only disadvantage to using the BSY bits is they have to be polled, rather than wait for a PIE Interrupt as with the INT_SEQ1/2 bits.  If customer was polling the SEQ1/2 anyway than this is a non-issue.

     

    Best,

    Matthew