Dear Champs, The F2833x reference design (sprc541) shows the interface between the F2833x and anASRAM (please refer to page 4 of the schematics or to the following figure): As far as I understand, the address lines (XA0-XA16) should be connected to thecorrespondent lines (A0-A16) in the ASRAM, however they are connected as follows: XA[0..8] <=> A [0..8] XA[9..15] <=> A[11..17] XA16 <=> A9 A10 is connected to ground. Is this the way it should be?