Other Parts Discussed in Thread: SM320F28335-EP
Hello,
I am using SM320F28335-EP Microcontroller. My question about the accuracy of the internal ADC. I want accuracy the of 10mV. But I am considering all the as per the below calculation and I am achieving the worst possible error of 24mV.
Per the datasheet the INL =1.5LSB, DNL=1LSB, Offset(Zero code) = 15LSB, Gain error = 30LSB over the operting range.
I added all the possible error and i am getting
| V Ref | 2.048 | V | ||
| Resolution | 12 | Bits | ||
| Number of steps | 4095 | |||
| V resolution | 0.5001221 | mV | ||
| Zero code error | 15 | LSB | 7.50183 | mV |
| Gain error | 30 | LSB | 15.0037 | mV |
| Linearity error (INL) | 2 | LSB | 1.00024 | mV |
| Total possible error | 24.00586081 | mV |
Please let me know how accurate this microcontroller is and how to tackle this problem. Or i need to use external ADC for this precise application.
Expecting earliest help from someone who worked on this processor.
Regards,
Manikandan.M