Hello,
I'm looking for a solution for controlling the Faulhaber 3564 servo motor (12 V, < 3,7A, /w Hall sensors). I think that the DRV8312-C2-KIT looks interesting for evaluation. My question is if the F28035 controller also can handle two BLDC motors. A setup with one BLDC and one stepper motor would also be interesting.
What are the advantages/disadvantages with the Piccolo in comparison with the other featured MCUs for BLDC control (Stellaris, MSP430)?
Do the DRV8312-C2-KIT handle sensored control "out of the box"?
Best Regards,
Johan