This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

New board startup problem



I have a new board with the Concerto chip installed. I have been able to download using XDS100V2 feature of CCS v4.2.5 and an on-board USB interface that is identical to the evaluation board (F28M35xx ISO Control Card). I have loaded blinky on both the new and the eval board. I get no response form the new board. The registers for both cases are shown below:

Any help would be greatly appreciated. What should be my next step?

Thanks,

Pat

 

Working eval board:

TI eval f28m35xx registers – good

Core Registers

            PC = 0x00205922

            SP = 0x200001B0

            LR = 0x00205909

            xPSR = 0x01000000

                        N = 0x0

                        Z = 0x0

                        C = 0x0

                        V = 0x0

                        Q = 0x0

                        ICI/IT_2 = 0x0

                        T = 0x1

                        RESV = 0x0

                        ICI/IT_1 = 0x0

                        RESV2 = 0x0

                        EXCEPTION = 0x0

            R0 = 0x00150D99

            R1 = 0x001E8480

            R2 = 0x000000FF

            R3 = 0x00000080

            R4 = 0x00000000

            R5 = 0x00000000

            R6 = 0x00000000

            R7 = 0x200001B8

            R8 = 0x00000000

            R9 = 0x00000000

            R10 = 0x00000000

            R11 = 0x00000000

            R12 = 0x400FB73C

            R13 = 0x200001B0

            R14 = 0x00205909

            MSP = 0x200001B0

            PSP = 0x00000000

            DSP = 0x00000000

            CTRL_FAULT_BASE_PRI = 0x00000000

                        CONTROL = 0x0

                        FAULTMASK = 0x0

                        BASEPRI = 0x0

                        PRIMASK = 0x0

 

And the failed board:

CCUV6 fail

Core Registers

            PC = 0x010013E0

            SP = 0x200048CC

            LR = 0x010013B9

            xPSR = 0x61000000

                        N = 0x0

                        Z = 0x1

                        C = 0x1

                        V = 0x0

                       Q = 0x0

                        ICI/IT_2 = 0x0

                        T = 0x1

                        RESV = 0x0

                        ICI/IT_1 = 0x0

                        RESV2 = 0x0

                        EXCEPTION = 0x0

            R0 = 0x40020804

            R1 = 0x00000001

            R2 = 0x00000011

            R3 = 0xFFFFFFFF

            R4 = 0x00000000

            R5 = 0x00000000

            R6 = 0x00000000

           R7 = 0x00000000

            R8 = 0x00000000

            R9 = 0x00000000

            R10 = 0x00000000

            R11 = 0x00000000

            R12 = 0x00000000

            R13 = 0x200048CC

            R14 = 0x010013B9

            MSP = 0x200048CC

            PSP = 0x00000000

            DSP = 0x00000000

            CTRL_FAULT_BASE_PRI = 0x00000000

                        null

                        null

                        null

                        null