This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problems to start with the PSIM Tutorial on SimCoder



Hello,

I've been struggling with this issue for few days. I'm new on this technology and for sure there are some tricks I should learn. 

First of all, I bought the C2000 Experimenter Kit with the aim to utilize for control on my power conversion projects. Also I have the PSIM 9.1 and I began to explore the benefits from the SimCoder in the CCS v.5.

The first issue on that tutorial (besides that still the same old CCS example as the PSIM 9.0 documents) is that the target is the TMDSDCDC2KIT. Afterwards, to import the project it is necessary to import as Legacy project *. pjt (not just as Project->Open as indicated by the tutorial).

So I got a warning: Invalid project path: Include path not found (\packages\ti\xdais). I found around here that if I remove it wont have any harm on the further operations (Properties->Include Options->Add dir and erase the offender path). The warning is gone, so far so good.

Then I proceed to build it and I received a bunch of errors and warnings (Console log attached)  i.e:

#10010 errors encountered during linking; "D:/Progs/Psim/1-ch dc-dc buck (C code)/1_ch_dc_dc_buck/../RamDebug/1_ch_dc_dc_buck.out" not built.

#10056 symbol "_PS_DelayMs" redefined: first defined in "D:/Progs/Psim/1-ch dc-dc buck (C code)/PsBiosRam.lib<SysInit.obj>"; redefined in "D:/Progs/Psim/1-ch dc-dc buck (C code)/PsBiosFlash.lib<SysInit.obj>"

#10263 F28335_FLASH_Lnk.cmd

#10263 F28335_FLASH_RAM_Lnk.cmd

#10264 F28335_FLASH_Lnk.cmd

#10264 F28335_FLASH_RAM_Lnk.cmd

I changed Compiler versions (from 6.1.1 to 5.2.12 and 5.1.6) with worst results.

There is a more accurate tutorial for this case (I'm wondering that the C coding is due)?  Did someone make it work/tried with CCS v5? Some suggestions to make it work? Am I doing something wrong?

Thank you for your assistance.

**** Build of configuration 1_RamDebug for project 1_ch_dc_dc_buck ****

C:\ti\ccsv5\utils\bin\gmake -k all 
'Building file: D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/1_ch_dc_dc_buck.c'
'Invoking: C2000 Compiler'
"C:/ti/ccsv5/tools/compiler/c2000_6.1.1/bin/cl2000" -v28 -ml --float_support=fpu32 -g --include_path="C:/ti/ccsv5/tools/compiler/c2000_6.1.1/include" --define="_DEBUG" --define="LARGE_MODEL" --diag_warning=225 --display_error_number --issue_remarks --diag_wrap=off -k --asm_directory="D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/RamDebug" --obj_directory="D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/RamDebug" --preproc_with_compile --preproc_dependency="1_ch_dc_dc_buck.pp"  "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/1_ch_dc_dc_buck.c"
'Finished building: D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/1_ch_dc_dc_buck.c'
' '
'Building file: D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/passwords.asm'
'Invoking: C2000 Compiler'
"C:/ti/ccsv5/tools/compiler/c2000_6.1.1/bin/cl2000" -v28 -ml --float_support=fpu32 -g --include_path="C:/ti/ccsv5/tools/compiler/c2000_6.1.1/include" --define="_DEBUG" --define="LARGE_MODEL" --diag_warning=225 --display_error_number --issue_remarks --diag_wrap=off -k --asm_directory="D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/RamDebug" --obj_directory="D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/RamDebug" --preproc_with_compile --preproc_dependency="passwords.pp"  "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/passwords.asm"
'Finished building: D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/passwords.asm'
' '
'Building target: D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/1_ch_dc_dc_buck/../RamDebug/1_ch_dc_dc_buck.out'
'Invoking: C2000 Linker'
"C:/ti/ccsv5/tools/compiler/c2000_6.1.1/bin/cl2000" -v28 -ml --float_support=fpu32 -g --define="_DEBUG" --define="LARGE_MODEL" --diag_warning=225 --display_error_number --issue_remarks --diag_wrap=off -k --asm_directory="D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/RamDebug" --obj_directory="D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/RamDebug" -z --stack_size=0x7b0 -m"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/RamDebug/1_ch_dc_dc_buck.map" --warn_sections -i"C:/ti/ccsv5/tools/compiler/c2000_6.1.1/lib" -i"C:/ti/ccsv5/tools/compiler/c2000_6.1.1/include" -i"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/1_ch_dc_dc_buck" -i"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)" --reread_libs --priority --display_error_number --diag_wrap=off --entry_point=code_start --rom_model -o "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/1_ch_dc_dc_buck/../RamDebug/1_ch_dc_dc_buck.out"  "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/DSP2833x_Headers_nonBIOS.cmd" "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_RAM_Lnk.cmd" "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/PsBiosRam.lib" "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/C28x_FPU_FastRTS_beta1.lib" "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/RamDebug/passwords.obj" "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/RamDebug/1_ch_dc_dc_buck.obj" -l"rts2800_fpu32.lib" "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_Lnk.cmd" "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd" "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/PsBiosFlash.lib" 
<Linking>
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_Lnk.cmd", line 8: error #10263: 
   RAML0 memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_Lnk.cmd", line 8: error #10264: 
   RAML0 memory range overlaps existing memory range RAML0
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_Lnk.cmd", line 10: error #10263: 
   ZONE7A memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_Lnk.cmd", line 10: error #10264: 
   ZONE7A memory range overlaps existing memory range ZONE7A
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_Lnk.cmd", line 11: error #10263: 
   FLASH_ALL memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_Lnk.cmd", line 11: error #10264: 
   FLASH_ALL memory range overlaps existing memory range FLASH_ALL
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_Lnk.cmd", line 12: error #10263: 
   CSM_RSVD memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_Lnk.cmd", line 12: error #10264: 
   CSM_RSVD memory range overlaps existing memory range CSM_RSVD
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_Lnk.cmd", line 13: error #10263: 
   BEGIN memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_Lnk.cmd", line 14: error #10264: 
   PASSWORDS memory range overlaps existing memory range CSM_PWL
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_Lnk.cmd", line 16: error #10263: 
   ADC_CAL memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_Lnk.cmd", line 16: error #10264: 
   ADC_CAL memory range overlaps existing memory range ADC_CAL
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_Lnk.cmd", line 18: error #10263: 
   IQTABLES memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_Lnk.cmd", line 18: error #10264: 
   IQTABLES memory range overlaps existing memory range IQTABLES
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_Lnk.cmd", line 19: error #10263: 
   IQTABLES2 memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_Lnk.cmd", line 19: error #10264: 
   IQTABLES2 memory range overlaps existing memory range IQTABLES2
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_Lnk.cmd", line 20: error #10263: 
   FPUTABLES memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_Lnk.cmd", line 20: error #10264: 
   FPUTABLES memory range overlaps existing memory range FPUTABLES
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_Lnk.cmd", line 21: error #10263: 
   BOOTROM memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_Lnk.cmd", line 21: error #10264: 
   BOOTROM memory range overlaps existing memory range BOOTROM
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_Lnk.cmd", line 22: error #10263: 
   RESET memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_Lnk.cmd", line 22: error #10264: 
   RESET memory range overlaps existing memory range RESET
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_Lnk.cmd", line 30: error #10263: 
   RAMM0 memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_Lnk.cmd", line 30: error #10264: 
   RAMM0 memory range overlaps existing memory range RAMM0
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_Lnk.cmd", line 32: error #10263: 
   ZONE7B memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_Lnk.cmd", line 32: error #10264: 
   ZONE7B memory range overlaps existing memory range ZONE7B
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 11: error #10263: 
   BOOT_RSVD memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 11: error #10264: 
   BOOT_RSVD memory range overlaps existing memory range BOOT_RSVD
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 13: error #10263: 
   RAML0 memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 13: error #10264: 
   RAML0 memory range overlaps existing memory range RAML0
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 13: error #10263: 
   RAML0 memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 13: error #10264: 
   RAML0 memory range overlaps existing memory range RAML0
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 14: error #10263: 
   ZONE7A memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 14: error #10264: 
   ZONE7A memory range overlaps existing memory range ZONE7A
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 14: error #10263: 
   ZONE7A memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 14: error #10264: 
   ZONE7A memory range overlaps existing memory range ZONE7A
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 15: error #10263: 
   FLASH_ALL memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 15: error #10264: 
   FLASH_ALL memory range overlaps existing memory range FLASH_ALL
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 15: error #10263: 
   FLASH_ALL memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 15: error #10264: 
   FLASH_ALL memory range overlaps existing memory range FLASH_ALL
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 16: error #10263: 
   CSM_RSVD memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 16: error #10264: 
   CSM_RSVD memory range overlaps existing memory range CSM_RSVD
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 16: error #10263: 
   CSM_RSVD memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 16: error #10264: 
   CSM_RSVD memory range overlaps existing memory range CSM_RSVD
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 17: error #10264: 
   CSM_PWL memory range overlaps existing memory range PASSWORDS
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 17: error #10263: 
   CSM_PWL memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 17: error #10264: 
   CSM_PWL memory range overlaps existing memory range CSM_PWL
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 18: error #10263: 
   ADC_CAL memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 18: error #10264: 
   ADC_CAL memory range overlaps existing memory range ADC_CAL
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 18: error #10263: 
   ADC_CAL memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 18: error #10264: 
   ADC_CAL memory range overlaps existing memory range ADC_CAL
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 19: error #10263: 
   RESET memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 19: error #10264: 
   RESET memory range overlaps existing memory range RESET
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 19: error #10263: 
   RESET memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 19: error #10264: 
   RESET memory range overlaps existing memory range RESET
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 20: error #10264: 
   BEGIN_FLASH memory range overlaps existing memory range BEGIN
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 21: error #10263: 
   IQTABLES memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 21: error #10264: 
   IQTABLES memory range overlaps existing memory range IQTABLES
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 21: error #10263: 
   IQTABLES memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 21: error #10264: 
   IQTABLES memory range overlaps existing memory range IQTABLES
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 22: error #10263: 
   IQTABLES2 memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 22: error #10264: 
   IQTABLES2 memory range overlaps existing memory range IQTABLES2
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 22: error #10263: 
   IQTABLES2 memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 22: error #10264: 
   IQTABLES2 memory range overlaps existing memory range IQTABLES2
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 23: error #10263: 
   FPUTABLES memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 23: error #10264: 
   FPUTABLES memory range overlaps existing memory range FPUTABLES
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 23: error #10263: 
   FPUTABLES memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 23: error #10264: 
   FPUTABLES memory range overlaps existing memory range FPUTABLES
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 24: error #10263: 
   BOOTROM memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 24: error #10264: 
   BOOTROM memory range overlaps existing memory range BOOTROM
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 24: error #10263: 
   BOOTROM memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 24: error #10264: 
   BOOTROM memory range overlaps existing memory range BOOTROM
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 28: error #10263: 
   RAMM0 memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 28: error #10264: 
   RAMM0 memory range overlaps existing memory range RAMM0
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 28: error #10263: 
   RAMM0 memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 28: error #10264: 
   RAMM0 memory range overlaps existing memory range RAMM0
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 29: error #10263: 
   ZONE7B memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 29: error #10264: 
   ZONE7B memory range overlaps existing memory range ZONE7B
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 29: error #10263: 
   ZONE7B memory range has already been specified
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 29: error #10264: 
   ZONE7B memory range overlaps existing memory range ZONE7B
warning #16002-D: build attribute vendor section TI missing in "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/C28x_FPU_FastRTS_beta1.lib<div_f32.obj>": compatibility cannot be determined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 44: warning #10190-D: absolute symbol "_CinitLoadStart" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 45: warning #10190-D: absolute symbol "_CinitRunStart" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 46: warning #10190-D: absolute symbol "_CinitSize" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 49: warning #10190-D: absolute symbol "_TextLoadStart" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 50: warning #10190-D: absolute symbol "_TextRunStart" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 51: warning #10190-D: absolute symbol "_TextSize" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 54: warning #10190-D: absolute symbol "_PinitLoadStart" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 55: warning #10190-D: absolute symbol "_PinitRunStart" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 56: warning #10190-D: absolute symbol "_PinitSize" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 59: warning #10190-D: absolute symbol "_SwitchLoadStart" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 60: warning #10190-D: absolute symbol "_SwitchRunStart" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 61: warning #10190-D: absolute symbol "_SwitchSize" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 64: warning #10190-D: absolute symbol "_ConstLoadStart" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 65: warning #10190-D: absolute symbol "_ConstRunStart" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 66: warning #10190-D: absolute symbol "_ConstSize" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 69: warning #10190-D: absolute symbol "_EconstLoadStart" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 70: warning #10190-D: absolute symbol "_EconstRunStart" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 71: warning #10190-D: absolute symbol "_EconstSize" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 74: warning #10190-D: absolute symbol "_RamfuncsLoadStart" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 75: warning #10190-D: absolute symbol "_RamfuncsRunStart" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 76: warning #10190-D: absolute symbol "_RamfuncsSize" being redefined
error #10056: symbol "_PSI_GetLspClk" redefined: first defined in "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/PsBiosRam.lib<SysInit.obj>"; redefined in "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/PsBiosFlash.lib<SysInit.obj>"
error #10056: symbol "_PSD_CpuClock" redefined: first defined in "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/PsBiosRam.lib<SysInit.obj>"; redefined in "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/PsBiosFlash.lib<SysInit.obj>"
error #10056: symbol "_PSI_InitSysCtrl" redefined: first defined in "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/PsBiosRam.lib<SysInit.obj>"; redefined in "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/PsBiosFlash.lib<SysInit.obj>"
error #10056: symbol "_PSI_InitPLLCR" redefined: first defined in "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/PsBiosRam.lib<SysInit.obj>"; redefined in "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/PsBiosFlash.lib<SysInit.obj>"
error #10056: symbol "_PS_DelayMs" redefined: first defined in "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/PsBiosRam.lib<SysInit.obj>"; redefined in "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/PsBiosFlash.lib<SysInit.obj>"
error #10056: symbol "_PSI_InitPieVectTable" redefined: first defined in "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/PsBiosRam.lib<SysInit.obj>"; redefined in "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/PsBiosFlash.lib<SysInit.obj>"
error #10056: symbol "_PSI_ReservedISR" redefined: first defined in "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/PsBiosRam.lib<SysInit.obj>"; redefined in "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/PsBiosFlash.lib<SysInit.obj>"
error #10056: symbol "_PSI_InitPieCtrl" redefined: first defined in "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/PsBiosRam.lib<SysInit.obj>"; redefined in "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/PsBiosFlash.lib<SysInit.obj>"
error #10056: symbol "_PS_SysInit" redefined: first defined in "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/PsBiosRam.lib<SysInit.obj>"; redefined in "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/PsBiosFlash.lib<SysInit.obj>"
error #10056: symbol "_PS_DelayUs" redefined: first defined in "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/PsBiosRam.lib<SysInit.obj>"; redefined in "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/PsBiosFlash.lib<SysInit.obj>"
error #10056: symbol "_PSI_InitPeripheralClocks" redefined: first defined in "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/PsBiosRam.lib<SysInit.obj>"; redefined in "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/PsBiosFlash.lib<SysInit.obj>"
error #10056: symbol "_PSI_DisableDog" redefined: first defined in "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/PsBiosRam.lib<SysInit.obj>"; redefined in "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/PsBiosFlash.lib<SysInit.obj>"
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 44: warning #10190-D: absolute symbol "_CinitLoadStart" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 45: warning #10190-D: absolute symbol "_CinitRunStart" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 46: warning #10190-D: absolute symbol "_CinitSize" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 49: warning #10190-D: absolute symbol "_TextLoadStart" being redefined

"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 50: warning #10190-D: absolute symbol "_TextRunStart" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 51: warning #10190-D: absolute symbol "_TextSize" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 54: warning #10190-D: absolute symbol "_PinitLoadStart" being redefined
>> Compilation failure
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 55: warning #10190-D: absolute symbol "_PinitRunStart" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 56: warning #10190-D: absolute symbol "_PinitSize" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 59: warning #10190-D: absolute symbol "_SwitchLoadStart" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 60: warning #10190-D: absolute symbol "_SwitchRunStart" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 61: warning #10190-D: absolute symbol "_SwitchSize" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 64: warning #10190-D: absolute symbol "_ConstLoadStart" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 65: warning #10190-D: absolute symbol "_ConstRunStart" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 66: warning #10190-D: absolute symbol "_ConstSize" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 69: warning #10190-D: absolute symbol "_EconstLoadStart" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 70: warning #10190-D: absolute symbol "_EconstRunStart" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 71: warning #10190-D: absolute symbol "_EconstSize" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 74: warning #10190-D: absolute symbol "_RamfuncsLoadStart" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 75: warning #10190-D: absolute symbol "_RamfuncsRunStart" being redefined
"D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/F28335_FLASH_RAM_Lnk.cmd", line 76: warning #10190-D: absolute symbol "_RamfuncsSize" being redefined
warning #10063-D: entry-point symbol other than "_c_int00" specified:  "code_start"
error #10010: errors encountered during linking; "D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/1_ch_dc_dc_buck/../RamDebug/1_ch_dc_dc_buck.out" not built
gmake: *** [D:/Todo/Progs/Psim/1-ch dc-dc buck (C code)/1_ch_dc_dc_buck/../RamDebug/1_ch_dc_dc_buck.out] Error 1
gmake: Target `all' not remade because of errors.

**** Build Finished ****