I received the DRV8412 kit. The board is rev. G. Followed instructions given in the quick start guide with two brushed motors connected. Started GUI (crosshairs) and clicked "Enable Motor". The motors did not spin. Readme in the GUI folder says Rev G board should use v6 GUI. I can only find v2 and v9 GUI's. The GUI displayed "Connect" and "Updates ON". Fault light was green. DC Bus light was off with value 28.8 V showed. The supply voltage was checked with a DVM. It was 23.4 V. Any idea?
Thank you!