This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HVPM_Sensorless - math block version differences?

I am working on a project and successfully implemented HVACI_Scalar using the motor control math blocks version 1.1 and the drivers in f2803x_v1.2. I am now going to add HVPM_Sensorless to the project and see that there are newer versions of these available. I do see some small differences in the newer versions, but do they essentially function the same? Are there any bug fixes in these newer versions? I could not find any release notes on these newer versions of the motor control math block and drivers.

Thanks.