Hi,
I simply wonder how I can confirm the ADC sample rate for my TMS320F28335? Currently, I'm sampling at 12.5 MSPS according to the code, but I would like to know if this i correct. Previously I sampled a square wave of 3 MHz and counted the number of samples per wave (manually, only for about 10 waves). The result was around 11.8 MSPS. This is lower than 12.5 MSPS, so I would like to know if there are more precise measurement methods. If the square wave method is reliable, what may the reasons be for the lower sample rate?
Regards, Fredrik