This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

f28m35 watchdog1

I have set up watchdog 1 to reset the processor after a period of 1ms (500us in WDTLOAD). I then reload the WDTLOAD register everytime I 'kick' the watchdog.

The watchdog timer does not reload after the initial setup (I am leaving the protection off for debugging).

If I swop to watchdog 0, the code works fine, although it seems like it is running from a much faster clock?

(Solved the faster clock - Watchdog1 runs off OSCCLK and Watchdog0 off M3SSCLK!)

I have observed the timing delay for writes to watchdog 1 by physical delays as well as polling for WRC - through the debugger I see that WRC does not return to 1 after the initial setup?

  • I have a solution to the problem with WDT1.

    If you reset the Watchdog interrupt via a write to the WDTICR, the initial setup value in the WDTLOAD is loaded into WDTVALUE and the watchdog counts down from there again.

    I could not get the reload working by a direct write to WDTLOAD in WDT1 - which does work with WDT0.