hello there ....
i m trying to use the high voltage motor control + PFC kit on the said board, by default the M1 [J9] was populated while J12 wasnt populated by a jumper b/w 1 and middle pin.
the set up guide says to populate J12 and M1 [J9] shouldnt be ...
the long and short is ... i do am following the steps.
but the video tutorial of chris clearman (c2000 marketing) depicts that both red leds on the piccolo control flash cards should be blinking ! in my case only the first one does !
now when i start the gui and try to connect ... (after setting up connection) i get an error message ...
unhandled exception ... "access to com port 15 is denied"
(in my case the laptop port i m using has the said name ! ) ...
can anyone please help me and guide me for what should i do in this regard ... ?
the port is enabled ... i have checked ...
thanking you all in anticipation.