This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS v5.3 Graph tool

Hi,

I'm experience some strange behavior when using the graph tool in CCS v5.3. I'm running the DRV8312-C2-KIT to evaluate the control performance with steep ramps. In the attached graph I've plotted (using the exported data) the speed reference (target) and the speed feedback from a quadrature encoder. As you can see there are some abrupt jumps both in the target ramp and the measured signal. I however doubt that the graph shows real values in those cases. Has anyone seen something similar? Even if I use a instantaneous step as target (i.e. no ramp) I sometimes observe this kid of glitch in the logged data. Does it maybe have anything to do with sampling rate or buffer size?

BR, Johan