This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unable to find TDP for CCS 3.3 in RTRT 7.0



I want to do run time tracing using RTRT for dsp code developed in CCS environment, i have selected C Code Composer C6xx as TDP for the project. While building the project at the time of preprocessing it is giving error as

'cl6x' is not recognized as an internal or external command, operable program or batch file

How to overcome this problem.