Hi,
I just purchased a DRV8412-C2-KIT. I was going through the pdf document for Dual-axis Current control of brushed DC motor..
Level 1C (DRV8412 Test)
After verifying PWM_MACRO module in level 1a, the dual full-bridge hardware in the DRV8412 are tested by looking at the low pass filter outputs. For this purpose, set the variable DRV_RESET to 0 through the watch window and check the ADC_Vhb1 and ADC_Vhb2 schematic nodes using an oscilloscope. You will observe that the phase voltage dividers and waveform monitoring filters (R42 to 45 & C55 to 56) enable the generation of the waveform and ensure that the DRV8412 is working appropriately.
I am unable to find these test points on the DRV8412-c2-kit.
Pls help.
Regards
Raghu.