Other Parts Discussed in Thread: DRV8301
I am needing to control a axial flux motor for a E-bike. 2,000 rpm max with 48 volt dc @ 10 to 12 kw. I am trying to set it up as a attraction/repulsion. I am wanting a 3 phase controller with each phase to pulse width modulate (PWM) for power control and quickly invert when coil centers on magnet (switch to repulse). I am sure there are a few nano seconds not to crash the FET's. This is not rotating the field around the stator but stepping around. I am using the 3 phases in 3 offset coil sets to reduce the cogging.
I was looking at developers kits. I found:
DK-LM3S-DVR8312, DK-LM4F-DVR8312, TMDS1MTRPFCKIT, DVR8312-C2-KIT, DVR8301/2 base kit
Any of these? help me? or is ther another direction I should go? any help APPRECIATED!