This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MISO SPI issue



Hi guys I am using the F28335 and I am using the SPI to communicate with a M25P40-VMN6P (4 Mbit, Low Voltage, Serial Flash Memory With 40MHz SPI Bus Interface).  I am getting a weird issue that i can't seem to figure out.  For some reason the MISO line is riding high when it should be riding low.  This is a read command that i am sending to the flash to read whats in the memory.  When the line is high it returns all FF.  


But after I call a second write command followed by a second read command the SPI line drops to low and I am able to read the correct information.

 

Here is the code i use to initialize the GPIO ports:


GpioCtrlRegs.GPBPUD.bit.GPIO54 = 0; // Enable pull-up on GPIO54 (SPISIMOA)
GpioCtrlRegs.GPBQSEL2.bit.GPIO54 = 3; // Asynch input GPIO54 (SPISIMOA)
GpioCtrlRegs.GPBMUX2.bit.GPIO54 = 1; // Configure GPIO54 as SPISIMOA
GpioCtrlRegs.GPBDIR.bit.GPIO54 = 1; //set FRAM CS as out

GpioCtrlRegs.GPBPUD.bit.GPIO55 = 0; // Enable pull-up on GPIO55 (SPISOMIA)
GpioCtrlRegs.GPBQSEL2.bit.GPIO55 = 3; // Asynch input GPIO55 (SPISOMIA)
GpioCtrlRegs.GPBMUX2.bit.GPIO55 = 1; // Configure GPIO55 as SPISOMIA

GpioCtrlRegs.GPBPUD.bit.GPIO56 = 0; // Enable pull-up on GPIO56 (SPICLKA)

GpioCtrlRegs.GPBQSEL2.bit.GPIO56 = 3; // Asynch input GPIO56 (SPICLKA)
GpioCtrlRegs.GPBMUX2.bit.GPIO56 = 1; // Configure GPIO56 as SPICLKA
GpioCtrlRegs.GPBDIR.bit.GPIO56 = 1; //set FRAM CS as out

GpioDataRegs.GPBSET.bit.GPIO57 = 1; //pre-set FRAM CS high
GpioCtrlRegs.GPBDIR.bit.GPIO57 = 1; //set FRAM CS as out
GpioDataRegs.GPBSET.bit.GPIO58 = 1; //pre-set EEP CS high
GpioCtrlRegs.GPBDIR.bit.GPIO58 = 1; //set EEP CS as out

Here is what is used for a write command to memory:

// SPI_Write:
//---------------------------------------------------------------------------
// This function executes a write, mode 1, on the SPI
//
void SPI_Write(Uint16 CS, Uint16 WA[4],Uint16 WA_count,Uint16 *dp,Uint16 data_length){
//---------------------------------------------------------------------------
// #ifdef RELEASE
Uint16 bs;
Uint16 j;
Uint16 i=0;
// char tempp[1];//trying to find out what CS is
// tempp[0]=CS;//trying to find out what CS is

// if(CS != 0x57 & CS !=0x58){
// SciaTx(tempp);//trying to find out what CS is
if(CS != 57 & CS !=58 & CS!=19 & CS!=15 & CS!=23 ){
SciaTx(String_err);
SciaTx(": Invalid CS");
return;
}
Msg_Flags.bit.Timeout = 0;
CS_Low(CS);

Msg_Flags.bit.spia_rx_rdy = 0;
bs = SpiaRegs.SPIRXBUF; //dummy read to clear int
SpiaRegs.SPIDAT = SPI_WREN<<8;
CpuTimer0Regs.TCR.bit.TSS = 0; //start Timer0 to catch runaway while loop
while(Msg_Flags.bit.spia_rx_rdy != 1){
if(Msg_Flags.bit.Timeout == 1){
SciaTx(String_err);
SciaTx(": SPI Timeout");
return;
}
}
CpuTimer0Regs.TCR.bit.TSS = 0; //stop Timer0 since while successful
CpuTimer0Regs.TCR.bit.TRB = 1; //reload Timer0
CS_High(CS); //latch WREN

DELAY_US(1);

CS_Low(CS); //start data tx

bs = SpiaRegs.SPIRXBUF; //dummy read to clear int
SpiaRegs.SPIDAT = SPI_WRITE<<8;
Msg_Flags.bit.spia_rx_rdy = 0;
bs = SpiaRegs.SPIRXBUF; //dummy read to clear int
CpuTimer0Regs.TCR.bit.TSS = 0; //start Timer0 to catch runaway while loop
while(Msg_Flags.bit.spia_rx_rdy != 1){
if(Msg_Flags.bit.Timeout == 1){
SciaTx(String_err);
SciaTx(": SPI Timeout");
return;
}
}
CpuTimer0Regs.TCR.bit.TSS = 0; //stop Timer0 since while successful
CpuTimer0Regs.TCR.bit.TRB = 1; //reload Timer0
// SpiaRegs.SPICCR.bit.SPICHAR = 0xF; //set to 16 bit mode
for(j=0;j<WA_count;j++){
SpiaRegs.SPITXBUF = WA[j]<<8;
Msg_Flags.bit.spia_rx_rdy = 0;
SpiaRegs.SPIFFRX.bit.RXFFINTCLR = 1;
bs = SpiaRegs.SPIRXBUF; //dummy read to clear int
CpuTimer0Regs.TCR.bit.TSS = 0; //start Timer0 to catch runaway while loop
while(Msg_Flags.bit.spia_rx_rdy != 1){
if(Msg_Flags.bit.Timeout == 1){
SciaTx(String_err);
SciaTx(": SPI Timeout");
return;
}
}
CpuTimer0Regs.TCR.bit.TSS = 0; //stop Timer0 since while successful
CpuTimer0Regs.TCR.bit.TRB = 1; //reload Timer0

}
// SpiaRegs.SPICCR.bit.SPICHAR = 0x7; //set to 8 bit mode

while(i<data_length)

{
if(SpiaRegs.SPISTS.bit.BUFFULL_FLAG !=1){
bs = *dp++;
SpiaRegs.SPITXBUF = bs<<8;
i++;
}
}
if(data_length < 2)
{
Msg_Flags.bit.spia_rx_rdy = 0;
SpiaRegs.SPIFFRX.bit.RXFFINTCLR = 1;
bs = SpiaRegs.SPIRXBUF; //dummy read to clear int
CpuTimer0Regs.TCR.bit.TSS = 0; //start Timer0 to catch runaway while loop
while(Msg_Flags.bit.spia_rx_rdy != 1){
if(Msg_Flags.bit.Timeout == 1){
SciaTx(String_err);
SciaTx(": SPI Timeout");
return;
}
}
CpuTimer0Regs.TCR.bit.TSS = 0; //stop Timer0 since while successful
CpuTimer0Regs.TCR.bit.TRB = 1; //reload Timer0
}

else
{
for(i=0;i<2;i++){ //wait for the last 2 data to be sent
Msg_Flags.bit.spia_rx_rdy = 0;
SpiaRegs.SPIFFRX.bit.RXFFINTCLR = 1;
bs = SpiaRegs.SPIRXBUF; //dummy read to clear int
CpuTimer0Regs.TCR.bit.TSS = 0; //start Timer0 to catch runaway while loop
while(Msg_Flags.bit.spia_rx_rdy != 1){
if(Msg_Flags.bit.Timeout == 1){
SciaTx(String_err);
SciaTx(": SPI Timeout");
return;
}
}
CpuTimer0Regs.TCR.bit.TSS = 0; //stop Timer0 since while successful
CpuTimer0Regs.TCR.bit.TRB = 1; //reload Timer0
}
}
CS_High(CS); //raise CS for write done
SciaTxByte(data_length);

DELAY_US(5000L); //Time for EEP write

CS_Low(CS); //lower for write disable
SpiaRegs.SPIDAT = SPI_WRDI<<8;
Msg_Flags.bit.spia_rx_rdy = 0;
SpiaRegs.SPIFFRX.bit.RXFFINTCLR = 1;
bs = SpiaRegs.SPIRXBUF; //dummy read to clear int
CpuTimer0Regs.TCR.bit.TSS = 0; //start Timer0 to catch runaway while loop
while(Msg_Flags.bit.spia_rx_rdy != 1){
if(Msg_Flags.bit.Timeout == 1){
SciaTx(String_err);
SciaTx(": SPI Timeout");
return;
}
}
CpuTimer0Regs.TCR.bit.TSS = 0; //stop Timer0 since while successful
CpuTimer0Regs.TCR.bit.TRB = 1; //reload Timer0
CS_High(CS); //raise to latch write disable
//#endif
}

This is the command used to read whats in the buffer:

// SPI_Read:
//---------------------------------------------------------------------------
// This function executes a read, mode 1, on the SPI
//
void SPI_Read(Uint16 CS,Uint16 RA[4],Uint16 RA_count,Uint16 BN){
//---------------------------------------------------------------------------
// #ifdef RELEASE
Uint16 i=0;
Uint16 j;
Uint16 n;

Msg_Flags.bit.Timeout = 0;
if(CS != 57 & CS !=58 & CS!=19 & CS!=15 & CS!=23 ){
// if(CS != 0x57 & CS !=0x58){
SciaTx(String_err);
SciaTx(": Invalid CS");
return;
}

CS_Low(CS); //drop CS to start

Msg_Flags.bit.spia_rx_rdy = 0; //clear flag and interrupt
n = SpiaRegs.SPIRXBUF; //dummy read to clear int
SpiaRegs.SPIDAT = SPI_READ<<8; //send read command
CpuTimer0Regs.TCR.bit.TSS = 0; //start Timer0 to catch runaway while loop
while(Msg_Flags.bit.spia_rx_rdy != 1){
if(Msg_Flags.bit.Timeout == 1){
SciaTx(String_err);
SciaTx(": SPI Timeout");
return;
}
}
CpuTimer0Regs.TCR.bit.TSS = 0; //stop Timer0 since while successful
CpuTimer0Regs.TCR.bit.TRB = 1; //reload Timer0

// SpiaRegs.SPICCR.bit.SPICHAR = 0xF; //set to 16 bit mode
for(j=0;j<RA_count;j++){
Msg_Flags.bit.spia_rx_rdy = 0; //clear flag and interrupt
SpiaRegs.SPIFFRX.bit.RXFFINTCLR = 1;
n = SpiaRegs.SPIRXBUF; //dummy read to clear int
SpiaRegs.SPITXBUF = RA[j]<<8; //send read address
CpuTimer0Regs.TCR.bit.TSS = 0; //start Timer0 to catch runaway while loop
while(Msg_Flags.bit.spia_rx_rdy != 1){
if(Msg_Flags.bit.Timeout == 1){
SciaTx(String_err);
SciaTx(": SPI Timeout");
return;
}
}
CpuTimer0Regs.TCR.bit.TSS = 0; //stop Timer0 since while successful
CpuTimer0Regs.TCR.bit.TRB = 1; //reload Timer0
}

// SpiaRegs.SPICCR.bit.SPICHAR = 0x7; //set to 8 bit mode

while(i<BN){
Msg_Flags.bit.spia_rx_rdy = 0; //clear flag and interrupt
SpiaRegs.SPIFFRX.bit.RXFFINTCLR = 1;
n = SpiaRegs.SPIRXBUF; //dummy read to clear int
SpiaRegs.SPIDAT = 0x00; //dummy write
while(Msg_Flags.bit.spia_rx_rdy != 1){
CpuTimer0Regs.TCR.bit.TSS = 0; //start Timer0 to catch runaway while loop
while(Msg_Flags.bit.spia_rx_rdy != 1){
if(Msg_Flags.bit.Timeout == 1){
SciaTx(String_err);
SciaTx(": SPI Timeout");
return;
}
}
CpuTimer0Regs.TCR.bit.TSS = 0; //stop Timer0 since while successful
CpuTimer0Regs.TCR.bit.TRB = 1; //reload Timer0
}
Data[i] = SpiaRegs.SPIRXBUF;
i++;
}

CS_High(CS);//raise CS to finish

SciaTxByte(BN);
i = n; //dummy transfer to clear build
//#endif
}