Other Parts Discussed in Thread: CONTROLSUITE
Hi, I'm considering using a Concerto MCU for my motor control project because it already provides the ability to do almost everything I need from a peripheral standpoint (sd card interface, ethernet, etc), but it also looks like it should be able to run a 3-phase motor if an appropriate motor driver IC is used. Is there a way I can use the InstaSPIN project with a Concerto MCU?