This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335- Example cod for Remote Frame Transmission.



hello,

1)  Is there any example code for Remote Frame Transmission in TMS320F28335 controller.

or suggestion of mailbox configuration for Remote Frame Transmission and receive it in same mailbox also a great help.

2)  Can I use eCANa as Tx and eCANb as Rx of same  TMS320F28335.  Let me tell you that I am working with TMS320F28335 (TMDSDOCK28335) Delfino Experimenter Kit.

3)  Can anyone tell the physical connection of one or two TMS320F28335 controller with PC for transmission and reception of normal CAN msgs in detail.

Any answer of this questions would be great help.

Thanks in advance

Regards

Mehul