Hello,
I'm writing to EPwmxRegs.TBPRDM.all a Uint32 and I can't see the number I wrote in the actual register once the writing instruction is executed. I'm using the Cla-C compiler and executing the following:
EPwm1Regs.TBPRDM.all = 0x02585900;
After executing this line EPwm1Regs.TBPRDM.all in the "Expressions" window on the debug perspective is still showing the value used in the initialization of the register (at the beginning of the program), as if the write wouldn't have happened at all.
Any suggestions?
Thanks,
Lucas