Other Parts Discussed in Thread: TMDSHVMTRINSPIN, MOTORWARE, CONTROLSUITE, CCSTUDIO
after noticing that there is an similar development kit TMDSHVMTRINSPIN, as TMDSHVMTRPFCKIT is, so I got a problem with choosing which one is better for my application, thus I've placed few basic questions. Please help me!
I have to make a choice between two kits:
TMDSHVMTRPFCKIT and TMDSHVMTRINSPIN, now I have following questions:
1. Is the TMDSHVMTRINSPIN kit comming with Code Composer Studio CD?
2. Can I use TMDSHVMTRINSPIN with delfino F28335 control card?
3. Is the TMDSHVMTRINSPIN equiped with output phases voltage sensors?
4. am I right that the difference between TMDSHVMTRINSPIN and TMDSHVMTRPFCKIT is only the control cards on it, is it the same power module?
Thank You!