This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335 8192 points fft

Hi Expert,

We are using 28335 to do 8192 points fft. But 28335 has 34K X 16 bits internal memory which are not enough to run the CFFT_f32 function with 8192 points. External memory is very slow and around 0.3 second per call. We used to have 8192 fft program which can do same input/output buffer 8192 fft on VC33.

Does 28335 have similar fft program (same in/out buffer) to meet our requirement?

thanks,