I am getting ready to use the SCI ports on the C28 section of my M36 and found descriptions of registers for two SCIs, A and B in the Technical Reference Manual. There is a note saying that B is not available on all chips. The main function diagram in the datasheet shows 1 SCI. But in the datasheet for the M36 parts on page 74, C28X Peripheral Mode 1 there are two pins for the SCIRXDA and two for the SCITXDA as follows:
SCIRXDA PE4_GPIO28 PF4_GPIO36
SCITXDA PE5_GPIO29 PF3_GPIO35
Does this mean there are two outputs and two inputs for the peripheral in the same mode? Or is this a typo and there are two ports available? Finally, if I am using C28 mode 1 which is the correct pin set to connect my level shifters to?