Other Parts Discussed in Thread: TMS320F28069
Hi,
I am planning on using your TMS320F28069 controller on my upcoming design and I have a couple questions about this part that I am having trouble finding in the datasheets and application notes. My first question is how to size the decoupling capacitors for the Vddio pins (I am planning on using the internal regulator on this chip for the vdd pins if that makes a difference). I was also curious if I could get a little better explanation on the behavior of the /XRS pin. In the datasheet it specifies that an R-C circuit should be connected to this pin for noise immunity, but I have had toruble finding any notes on how to size this filter. I was also curious about the POR and BOR function on this chip. On the previous design I have a reset chip that is 2.93V, open collector, and active low connected to this pin and I plan to do the same thing on this one. I was wondering how the reset chip would react with the POR and BOR and if I use a 10K pull up resistor, could this result in too much current flowing through this pin?
Thanks