Other Parts Discussed in Thread: TMS320F28027
I am working on a TMDSSOLARPEXPKIT for running a full pv inverter system. I tried to flash the PV emulation code to the TMS320F28027 Piccolo controller from the example projects available in the control suite but it says my device is held on reset and i need to take the device out of reset. Provide suggestion towards taking the kit out of reset.
Following is the error shown on debugging the code.
C28xx: Error enabling realtime mode: (Error -2134 @ 0x0) Unable to control device execution state. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.0.681.0)
C28xx: Trouble Reading PC Register: (Error -1137 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 5.0.681.0)
C28xx: Trouble Reading Register RPC: (Error -1137 @ 0x13) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 5.0.681.0)
Thanks,
Abdullah