Other Parts Discussed in Thread: CONTROLSUITE
Good day.
ControlSUITE download page says that it supports TMS320F280x but it doesn't (reference link from F2808 software download section).
I really excited of new style API for peripherals and system for F2802x and have adopted this API for F280x and make it available on https://github.com/ya-mouse/f280x_driverlib.
I've found a mistake in v210/f2802x_common/source/sci.c in Register name that makes it unusable:
void SCI_setRxFifoIntLevel(SCI_Handle sciHandle, const SCI_FifoLevel_e fifoLevel) { SCI_Obj *sci = (SCI_Obj *)sciHandle; // clear the value sci->SCIFFTX &= (~SCI_SCIFFRX_IL_BITS); // set the bits sci->SCIFFRX |= fifoLevel; return; } // end of SCI_setRxFifoIntLevel() function |
In a polling mode initialized as follows:
| CLK_enableSciaClock(myClk); /* 1 stop bit, No loopback * No parity,8 char bits, * async mode, idle-line protocol */ SCI_disableParity(mySci); SCI_setNumStopBits(mySci, SCI_NumStopBits_One); SCI_setCharLength(mySci, SCI_CharLength_8_Bits); /* enable TX, RX, internal SCICLK, * Disable RX ERR, SLEEP, TXWAKE */ SCI_enableTx(mySci); SCI_enableRx(mySci); SCI_enableTxInt(mySci); SCI_enableRxInt(mySci); /* SCI BRR = LSPCLK/(SCI BAUDx8) - 1 */ /* SciaRegs.SCIHBAUD = 0x00; */ /* (CPU_FRQ / (115200 * 32) - 1) */ /* SciaRegs.SCILBAUD = 0x1b; */ /* 9600 baud == 0x144 @ 100MHz SYSCLOCKOUT; */ SCI_setBaudRate(mySci, SCI_BaudRate_115_2_kBaud); SCI_enable(mySci); /* Setup SCI-A FIFO */ SCI_enableFifoEnh(mySci); SCI_resetTxFifo(mySci); SCI_clearTxFifoInt(mySci); SCI_resetChannels(mySci); SCI_setTxFifoIntLevel(mySci, SCI_FifoLevel_1_Word); SCI_enableTxFifoInt(mySci); SCI_resetRxFifo(mySci); SCI_clearRxFifoInt(mySci); SCI_setRxFifoIntLevel(mySci, SCI_FifoLevel_1_Word); SCI_enableRxFifoInt(mySci); |
I was unable to receive anything while SCI_isRxDataReady() checks for SCI_SCIRXST_RXRDY_BITS in SCIRXST register. I've changed this check to SCI_SCIFFRX_FIFO_ST_BITS in SCIFFRX register to get it works.
Also there is a mistype in sprs230n.pdf, page 46, table 3-15 in line:
| Reserved | 0x701F – 0x7020 | 1 | Reserved |
Column "size" should be equal to "2".