This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XINTF interface on 28335



I have two 28335 devices (say A and B) in a single system and need to share information between them at a high speed. Can the XINTF interface be used for this purpose? Is there a slave mode on the XINTF interface? i.e use A in master mode and B is slave mode so that A can read and write to B's RAM?

If not, how else can we share information between the two processors?

In the system, some analog inputs are connected to A and some to B. B has to pass the ADC readings to A.

Any ideas?